how to make H750 run a code more than 300KByte,at high speed。
i have a project want to use stm32h750。
but flash stm32h750 is small,just 128Kbytes,and my code is as much as 300Kbytes。
so i think i have two way :
1�?connect a extern flash by Quad-SPI,burn my program in extern flash,and boot from address—0x90000000。but worried about reducing the efficiency of code execution。
so if boot from extern flash,the set clock is 480MHz,the DMIPS Value is?
2�?the other method is——every time after power on,move code from extern flash,to internal ram,then boot from ram。
so,is there any example available?