Question
When an STM32 microcontroller is debuged, the probram being debugged is stored in the Flash?
Hello,
When an STM32 microcontroller is debugged using ST-LINK and STM32CubeID, the program that is being debug is burn in the Flash?
In other words, when I debug a program in STM32 microcontroller, the program previously stored in the Flash is overwritten?
To sum up. My doubt is about if I can flash the microcontroller through STM32CubeIDE or it is necessary using the programing utility to flash the STM32.
Regards,