Question
BMP280 I2C is not updating
Hi,
I am using stm32l432kc nucleo and BMP280 sensor with I2c communication.
During the debugging I realized that the data from the sensor is not updating, always 2481 (temp32 variable).
Could you help me in this topic?
Thank you in advance.
Info:
Used driver:
https://github.com/BoschSensortec/BMP280_driver
BMP280 application file:
#include "bmp280_defs.h"
#include "bmp280_user.h"
extern I2C_HandleTypeDef hi2c1;
HAL_StatusTypeDef status = HAL_OK;
/*!
* @brief Function that creates a mandatory delay required in some of the APIs such as "bmg250_soft_reset",
* "bmg250_set_foc", "bmg250_perform_self_test" and so on.
*
* @param[in] period_ms : the required wait time in milliseconds.
* @return void.
*
*/
void delay_ms(uint32_t period_ms)
{
HAL_Delay(period_ms);
}
/*!
* @brief Function for writing the sensor's registers through I2C bus.
*
* @param[in] i2c_addr : sensor I2C address.
* @param[in] reg_addr : Register address.
* @param[in] reg_data : Pointer to the data buffer whose value is to be written.
* @param[in] length : No of bytes to write.
*
* @return Status of execution
* @retval 0 -> Success
* @retval >0 -> Failure Info
*
*/
int8_t i2c_reg_write(uint8_t i2c_addr, uint8_t reg_addr, uint8_t *reg_data, uint16_t length)
{
int8_t rslt = BMP280_OK;
status = HAL_I2C_Mem_Write(&hi2c1, (uint8_t)(i2c_addr<<1), (uint8_t)reg_addr, I2C_MEMADD_SIZE_8BIT, (uint8_t*)(®_data), length, 10000);
if (status != HAL_OK)
{
rslt = BMP280_E_COMM_FAIL;
}
return rslt;
}
/*!
* @brief Function for reading the sensor's registers through I2C bus.
*
* @param[in] i2c_addr : Sensor I2C address.
* @param[in] reg_addr : Register address.
* @param[out] reg_data : Pointer to the data buffer to store the read data.
* @param[in] length : No of bytes to read.
*
* @return Status of execution
* @retval 0 -> Success
* @retval >0 -> Failure Info
*
*/
int8_t i2c_reg_read(uint8_t i2c_addr, uint8_t reg_addr, uint8_t *reg_data, uint16_t length)
{
int8_t rslt = BMP280_OK;
uint8_t array[28] = {0};
uint8_t stringpos = 0;
array[0] = reg_addr;
status = HAL_I2C_Mem_Read(&hi2c1, (uint8_t)(i2c_addr<<1), (uint8_t)reg_addr, I2C_MEMADD_SIZE_8BIT, (uint8_t*)(&array), length, 10000);
for (stringpos = 0; stringpos < length; stringpos++)
{
*(reg_data + stringpos) = array[stringpos];
}
if (status != HAL_OK)
{
rslt = BMP280_E_COMM_FAIL;
}
return rslt;
}main.c:
/**
******************************************************************************
* @file : main.c
* @brief : Main program body
******************************************************************************
* @attention
*
* <h2><center>© Copyright (c) 2020 STMicroelectronics.
* All rights reserved.</center></h2>
*
* This software component is licensed by ST under Ultimate Liberty license
* SLA0044, the "License"; You may not use this file except in compliance with
* the License. You may obtain a copy of the License at:
* www.st.com/SLA0044
*
******************************************************************************
*/
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "init.h"
#include "cmsis_os.h"
#include "Adafruit_INA219.h"
#include "bmp280.h"
#include "bmp280_user.h"
#include <stdio.h>
/* Private includes ----------------------------------------------------------*/
/* Private typedef -----------------------------------------------------------*/
/* Private define ------------------------------------------------------------*/
/* Private macro -------------------------------------------------------------*/
/* Private variables ---------------------------------------------------------*/
extern I2C_HandleTypeDef hi2c1;
extern UART_HandleTypeDef huart2;
// Task handles
//TaskHandle_t Task1HandleIna219 = NULL;
TaskHandle_t TanskHandleBmp280 = NULL;
/* Private function prototypes -----------------------------------------------*/
//static void Ina219(void * argument);
static void Bmp280(void * argument);
/* Private user code ---------------------------------------------------------*/
// data from INA219
//float current, busVoltage, shuntVoltage, power;
// data from BMP280
int8_t rslt;
struct bmp280_dev bmp;
struct bmp280_config conf;
struct bmp280_uncomp_data ucomp_data;
int32_t temp32;
double temp;
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* Configure the system clock */
SystemClock_Config();
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_I2C1_Init();
MX_USART2_UART_Init();
bmp.delay_ms = delay_ms;
bmp.dev_id = BMP280_I2C_ADDR_PRIM;
bmp.intf = BMP280_I2C_INTF;
bmp.read = i2c_reg_read;
bmp.write = i2c_reg_write;
rslt = bmp280_init(&bmp);
rslt = bmp280_get_config(&conf, &bmp);
conf.filter = BMP280_FILTER_COEFF_2;
conf.os_temp = BMP280_OS_4X;
conf.os_pres = BMP280_OS_NONE;
conf.odr = BMP280_ODR_1000_MS;
rslt = bmp280_set_config(&conf, &bmp);
rslt = bmp280_set_power_mode(BMP280_NORMAL_MODE, &bmp);
/* IN219 calibration */
//setCalibration_32V_1A();
/* Create the thread(s) */
//xTaskCreate(Ina219, "Ina219", configMINIMAL_STACK_SIZE, NULL, 0, &Task1HandleIna219);
xTaskCreate(Bmp280, "Bmp280", configMINIMAL_STACK_SIZE, NULL, 0, &TanskHandleBmp280);
/* Start scheduler */
vTaskStartScheduler();
/* We should never get here as control is now taken by the scheduler */
/* Infinite loop */
while (1)
{
}
}
/**
* @brief Ina219 thread.
* @param argument: Not used
* @retval
*/
/*static void Ina219(void * argument)
{
while(1)
{
// Show instantaneous measurements values
current = getCurrent_mA();
//busVoltage = getBusVoltage_V();
//shuntVoltage = getShuntVoltage_mV();
//power = getPower_mW();
printf("current = %.2f \n\r", current);
osDelay(1000);
}
}
*/
/**
* @brief Bmp280 thread.
* @param argument: Not used
* @retval
*/
static void Bmp280(void * argument)
{
while(1)
{
rslt = bmp280_get_uncomp_data(&ucomp_data, &bmp);
rslt = bmp280_get_comp_temp_32bit(&temp32, ucomp_data.uncomp_temp, &bmp);
rslt = bmp280_get_comp_temp_double(&temp, ucomp_data.uncomp_temp, &bmp);
printf("temp = %.f \n\r", temp);
vTaskDelay(1000);
taskYIELD();
}
}
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
if (htim->Instance == TIM1) {
HAL_IncTick();
}
}
/**
* @brief Retargets the C library printf function to the USART.
* @param None
* @retval None
*/
int fputc(int ch, FILE *f)
{
HAL_UART_Transmit(&huart2, (uint8_t *)&ch, 1, 0xFFFF);
return ch;
}
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* User can add his own implementation to report the HAL error return state */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(char *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
tex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/