Associate III
September 8, 2020
Solved
VL6180X INTERRUPT TO GPIO1
- September 8, 2020
- 8 replies
- 2811 views
Hello,
I am using a PNUCLEO VL6180X and I would like to drive my LED from the GPIO1 interrupt output only this output as shown in the diagrams above is always at 1 and it goes to 0 only for a few nanoseconds; I would like to have an interrupt signal only when I bring my hand closer to the sensor, I would like it to send a 1 to the LED when there is a target and a 0 when there is nothing.
Here are some images on the oscilloscope with the target and without the target