Skip to main content
Aabde.1
Associate
September 7, 2020
Question

for L9826 chip when apply 13v and "output shorted to Vbat" is detected , when remove this fault the output remain pulled high , so is there is any steps needed to be applied to recover from this failture ?

  • September 7, 2020
  • 4 replies
  • 953 views

..

This topic has been closed for replies.

4 replies

Peter BENSCH
ST Technical Moderator
September 8, 2020

Overload conditions are buffered as long as the L9826 is being powered.

After eliminating the cause of the fault you could do a reset using the pin NRes. With parallel control, special care is required at outputs 1 and 2, see section 5.2.1 of the datasheet.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Aabde.1
Aabde.1Author
Associate
September 8, 2020

Hello peter ,

thank you for reply ,

but if i am not using the parallel and i am using "Via 8-bit SPI " do i need to do reset also or the fault can be eliminated by other way,

take in consideration that when i apply a failure on a specific output pin and i remove this fault it can be eliminated if i flicker this pin one time so is that normal ?

Peter BENSCH
ST Technical Moderator
September 8, 2020

Sorry, I don't understand the last sentence. What do you mean with "flicker a pin"?

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.