Skip to main content
MStuc.1
Associate II
August 31, 2020
Question

Why clear the DMAR bit in UART DMA receive interrupt subroutine

  • August 31, 2020
  • 3 replies
  • 1079 views

Why should I clear the DMAR bit in the UART DMA receive interrupt subroutine?

At the moment I disable the DMA TC interrupt and the DMA Mode for reception (DMAR) at the top of my interrupt routine.

At the end of the subroutine I enable the uart dma receiver again.

This code works well.

But If I do not disable the DMA Mode for reception (DMAR) it does no longer work properly but I don't know why this makes such a difference?

Any thought on that topic?

Kind regards Mathias

This topic has been closed for replies.

3 replies

TDK
August 31, 2020

The answer to your question will depend on your code. You certainly don't need to clear it in general. If you're receiving a fixed length message, you should clear it and re-initialize the next transfer.

"If you feel a post has answered your question, please click ""Accept as Solution""."
MStuc.1
MStuc.1Author
Associate II
August 31, 2020

Thanks for the reply!

Yes, I receive a fixed length message. But still, why should I clear it. It is nothing written that this flag resets something?

waclawek.jan
Super User
August 31, 2020

> The answer to your question will depend on your code.

JW