Skip to main content
RZHU.1
Associate III
August 30, 2020
Solved

My on board ST link V3 cannot work?

  • August 30, 2020
  • 2 replies
  • 1125 views

The development board is STM32H757I-EVAL which has a ST link V3 on it,but after I download my program (just once) and update the firmware, it cannnot work correctly.

Here is the situation when I try to debug it:

0693W000002liNfQAI.png

This topic has been closed for replies.
Best answer by Tesla DeLorean

Jumper BOOT0 High, power cycle the board a couple of times, when STM32 Cube Programmer can attach, erase the device.

​

The check the LDO/SMPS and VOS configuration in your code, and if the debug port or pins are being disabled.​

2 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
August 30, 2020

Jumper BOOT0 High, power cycle the board a couple of times, when STM32 Cube Programmer can attach, erase the device.

​

The check the LDO/SMPS and VOS configuration in your code, and if the debug port or pins are being disabled.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
RZHU.1
RZHU.1Author
Associate III
August 30, 2020

Thanks so much!

I just switch the SW1 to set the boot0 HIGH, then it works!