MX_USB_DEVICE_Init() : VDDUSB presence not checked before removing power isolation
Hi,
I'm using CubeIDE 1.4.2 with CubeMX 6.0.1-RC3 and target is STM32L452.
This problem only occured with VDDUSB independent from VDD.
I had problems with USB FS device initialization (using CDC class but I guess it applies to other classes as well).
The problem was that after boot, when calling MX_USB_DEVICE_Init() with VDDUSB not present (usb not plugged in), the program was endlessly interrupted and stuck in USB_IRQHandler(), after calling USB_DevInit() in HAL_PCD_Init() in the file stm32l4xx_hal_pcd.c.
The problem never occured when VDDUSB was present (usb plugged in).
Here's the call hierachy :

Reading the Reference Manual RM0394, it's mentioned page 137 : 
As specified in the title, MX_USB_DEVICE_Init() never follows this sequence before removing the power isolation by setting the USV bit in PWR_CR2 by calling HAL_PWREx_EnableVddUSB(). The PVMO1 bit is never checked, which surely caused problems in further USBD initialization.
Call hierachy :

Checking if VDDUSB is present before calling MX_USB_DEVICE_Init() solved the thing.
Hope it can help someone.
(and maybe the check could be added in next version of CubeMX FW_L4 Package?
I'm using V1.15.1 here but I checked and it's still the same in V1.16.0)
Regards,
OE