Associate III
August 25, 2020
Question
Anybody else run into this error with STM32CubeMX? Any suggestions on how to fix it?
- August 25, 2020
- 3 replies
- 1783 views
I amusing STM32CubeMX version 6.0.1.
My board is based on the STM32L071RBT6 MCU.
I am using the IOC file attached to this post.
The code generator is configured for KEIL MDK 5.27 (same with MDK v5).
The code generator appears to complete successfully -- I get a pop up indicating the same.

However, when I click on either of the two options (Open Folder, Close) I get the same error popup shown below. I also notice that there is no startup or scatter load descriptor either