what is the the hardware fifo size of STM32f103CB and how to know whether the FIFO is empty or full?
Hi
As the title mentioned, I can't find relevant information in the datasheet.
I get some problem when using UART. I have two chips, the master chip transmits packages to RS485 Bus line, and the slave chip receives it then transmits the respond(UART1), at the same time, every second the timer will transmit debugging stuff to pc by TTL(UART2), they should be mutual independent, however the UART1 doesn't work when UART2 is working, and the data is still transmiting to RS485 bus from master chip, so some of the data will not received by slave chip when slave chip is using UART2, after a while whole system on slave chip get weird (the timer is still working), I guess it is the FIFO overflow. So I am asking for function or ways to know the fifo size remain.
Thanks.