Crystal Selection for the STM32H753AI
I am planning to connect a LSE 32kHz crystal and a 25MHz crystal to the HSE input, but I am having a hard time identifying whether the STM will drive my crystal selection within the limits of the 100uW drive level. I have read thru the app note, but it still isn't clear. The crystal I am using for the HSE is the ECS-250-8-33-JGN-TR. It has a 100uW drivel level maximum. Will this be compatible with the STM32H753?