Question
What is the maximum GPIO to memory DMA throughput on a STM32-H743ZI clocked at 480 MHz when running 1 or 2 channels simultaneously?
I would like to attach 2 high speed A/Ds connected via parallel GPIOs and run them at 50 MHz each, or 100 MHz aggregate. One A/D is 12 bit and the other is 8 bit so I could take advantage of FIFO packing on the memory side. The capture buffer size would be 10k for each channel.
Is this throughput possible? If so, what would be the best way to configure and trigger the 2 DMA channels?