Skip to main content
PSarr.1
Associate II
Aug 18, 2020 1:30 PM UTC
Question

FATFS + FreeRTOS memory corruption, need confirmation

Hi,

I created a project using the STM32CubeIDE for a STM32F2xx. This project include USB in host mode with a mass storage class, FATFS and FreeRTOS.

With freeRTOS, FATFS is put in REETRANT mode. I also put the MAX_SS to 4096 because I need the sector size to be bigger for a fafts-flash implementation.

When I do a f_mount, the fs->sobj is created and lock. In the f_mount function we called find_volume which then eventually call the function "USBH_ioctl" in usbh_ioctl to get the sector size.

The current implementation is casting the void * buff parameter to a DWORD *. But, in this case the void * buff is a pointer to (fs)->ssize which is a WORD.

So the current implementation is corrupting the fs->sobj which is place right after the ssize variable in the fs structure.

typedef struct {
 union{
	UINT	d32[_MAX_SS/4]; /* Force 32bits alignement */ 
	BYTE	d8[_MAX_SS];	/* Disk access window for Directory, FAT (and file data at tiny cfg) */ 
 }win;
	BYTE	fs_type;		/* FAT sub-type (0:Not mounted) */
	BYTE	drv;			/* Physical drive number */
	BYTE	csize;			/* Sectors per cluster (1,2,4...128) */
	BYTE	n_fats;			/* Number of FAT copies (1 or 2) */
	BYTE	wflag;			/* win[] flag (b0:dirty) */
	BYTE	fsi_flag;		/* FSINFO flags (b7:disabled, b0:dirty) */
	WORD	id;				/* File system mount ID */
	WORD	n_rootdir;		/* Number of root directory entries (FAT12/16) */
#if _MAX_SS != _MIN_SS
	WORD	ssize;			/* Bytes per sector (512, 1024, 2048 or 4096) */
#endif
#if _FS_REENTRANT
	_SYNC_t	sobj;			/* Identifier of sync object */
#endif
#if !_FS_READONLY
	DWORD	last_clust;		/* Last allocated cluster */
	DWORD	free_clust;		/* Number of free clusters */
#endif
#if _FS_RPATH
	DWORD	cdir;			/* Current directory start cluster (0:root) */
#endif
	DWORD	n_fatent;		/* Number of FAT entries, = number of clusters + 2 */
	DWORD	fsize;			/* Sectors per FAT */
	DWORD	volbase;		/* Volume start sector */
	DWORD	fatbase;		/* FAT start sector */
	DWORD	dirbase;		/* Root directory start sector (FAT32:Cluster#) */
	DWORD	database;		/* Data start sector */
	DWORD	winsect;		/* Current sector appearing in the win[] */
	
} FATFS;

Event the comment of the get_Sector_size is saying a WORD... see current code of USBH_ioctl() in usbh_diskio.c

 /* Get R/W sector size (WORD) */ 
 case GET_SECTOR_SIZE :	
 if(USBH_MSC_GetLUNInfo(&HOST_HANDLE, lun, &info) == USBH_OK)
 {
 *(DWORD*)buff = info.capacity.block_size;
 res = RES_OK;
 }
 else
 {
 res = RES_ERROR;
 }
 break;

If I make the following change, there is no more memory corruption

*(DWORD*)buff = info.capacity.block_size; -> *(WORD*)buff = info.capacity.block_size;

It can be me who doesn't use the library correctly... I would appreciate if somebody can confirm this problem and let me know the best way to get it corrected for everybody.

Let me know if you need more details

Regards

This topic has been closed for replies.