Skip to main content
MS.1134
Associate II
Aug 16, 2020 3:58 PM UTC
Solved

STM32F072-Disco_TSC_Resolution_Position Calculation on 3 Ch Touch Slider_touch key

To understand capacitive touch / TSC library based application, I’ve been studying the polling based sample code given in AN5105 for STM32F072B-Disco evaluation board. After tweaking the code to customize for the application, I’ve a few questions as below which I am not able to understand and can’t find any explanation even after reviewing various application notes from ST. Your input would be much appreciated and would be very helpful for me to clarify the concepts of TSC.

1. Resolution and Calculation of touch Position on the slider in the range of 0...255:

The header file, tsl_conf.h, supplied by TSC, has the following parameters:

#define TSLPRM_LINROT_RESOLUTION (7) //Position resolution in number of bits (range=1..8)

#define TSLPRM_USE_3CH_LIN_H (1) //Half ended electrode design

MyLinRots[0].p_Data->Position structure is used to compare the position value in the range of 0...255, but I am not able to understand the correlation of the value and position of touch on the slider / channel. How does Resolution value 1..8 affect this calculation?

Is there any formula based on resolution parameter to calculate position value

based on which channel is touched on the slider?

In the example code given in AN5105, I am trying to get 4 LEDs to be evenly distributed in the entire slider over the range of 0...255 with the following code, but not able to understand the calculation of the values used to compare with MyLinRots[0].p_Data->Position structure :

if(MyLinRots[0].p_Data->StateId == TSL_STATEID_DETECT)

{

//TSLPRM_LINROT_RESOLUTION

if(MyLinRots[0].p_Data->Position >= 1 && MyLinRots[0].p_Data->Position < 60)

{

HAL_GPIO_WritePin(LD4_GPIO_Port, LD3_Pin, GPIO_PIN_SET);

HAL_GPIO_WritePin(LD4_GPIO_Port, LD4_Pin, GPIO_PIN_RESET);

HAL_GPIO_WritePin(LD6_GPIO_Port, LD6_Pin, GPIO_PIN_RESET);

HAL_GPIO_WritePin(LD5_GPIO_Port, LD5_Pin, GPIO_PIN_RESET);

}

if(MyLinRots[0].p_Data->Position >= 60 && MyLinRots[0].p_Data->Position < 120)

{

HAL_GPIO_WritePin(LD4_GPIO_Port, LD3_Pin, GPIO_PIN_RESET);

HAL_GPIO_WritePin(LD6_GPIO_Port, LD6_Pin, GPIO_PIN_RESET);

HAL_GPIO_WritePin(LD4_GPIO_Port, LD4_Pin, GPIO_PIN_SET);

HAL_GPIO_WritePin(LD5_GPIO_Port, LD5_Pin, GPIO_PIN_RESET);

}

if(MyLinRots[0].p_Data->Position >= 120 && MyLinRots[0].p_Data->Position < 180)

{

HAL_GPIO_WritePin(LD4_GPIO_Port, LD3_Pin, GPIO_PIN_RESET);

HAL_GPIO_WritePin(LD5_GPIO_Port, LD5_Pin, GPIO_PIN_RESET);

HAL_GPIO_WritePin(LD4_GPIO_Port, LD4_Pin, GPIO_PIN_RESET);

HAL_GPIO_WritePin(LD6_GPIO_Port, LD6_Pin, GPIO_PIN_SET);

}

if(MyLinRots[0].p_Data->Position >= 180 && MyLinRots[0].p_Data->Position < 255)

{

HAL_GPIO_WritePin(LD4_GPIO_Port, LD3_Pin, GPIO_PIN_RESET);

HAL_GPIO_WritePin(LD5_GPIO_Port, LD5_Pin, GPIO_PIN_SET);

HAL_GPIO_WritePin(LD4_GPIO_Port, LD4_Pin, GPIO_PIN_RESET);

HAL_GPIO_WritePin(LD6_GPIO_Port, LD6_Pin, GPIO_PIN_RESET);

}

}

else

//if(MyLinRots[0].p_Data->StateId == TSL_STATEID_RELEASE)

{

HAL_GPIO_WritePin(LD4_GPIO_Port, LD3_Pin, GPIO_PIN_RESET);

HAL_GPIO_WritePin(LD4_GPIO_Port, LD4_Pin, GPIO_PIN_RESET);

HAL_GPIO_WritePin(LD5_GPIO_Port, LD5_Pin, GPIO_PIN_RESET);

HAL_GPIO_WritePin(LD6_GPIO_Port, LD6_Pin, GPIO_PIN_RESET);

}

2. In another example, I re-configured the touch channels on the same STM32F072B-Disco board as 3 individual touch keys. If I keep TSLPRM_TKEY_Detect_IN_TH and

TSLPRM_TKEY_Detect_OUT_TH parameters in tsl_conf.h header file as default of

110 & 120, the project compiles without any error.

// TouchKeys Detect state input threshold (range=0..255)

#define TSLPRM_TKEY_DETECT_IN_TH (110)

// TouchKeys Detect state output threshold (range=0..255)

#define TSLPRM_TKEY_DETECT_OUT_TH (120)

With these parameter values, I had to press very **** ** the channels and often times, it was very difficult to detect touch, so I reconfigured detect threshold to lower value of 50.

#define TSLPRM_TKEY_DETECT_IN_TH (50)

With this change, I get compiling errors as below:

../Middlewares/ST/STM32_TouchSensing_Library/inc/tsl_check_config.h(162):

error: #35: #error directive: "TSLPRM_TKEY_DETECT_OUT_TH is out of range

(TSLPRM_TKEY_PROX_IN_TH+1 .. TSLPRM_TKEY_DETECT_IN_TH-1)."

User code is as follow:

//Private macro

#define TEST_TKEY(NB)

((MyTKeys[(NB)].p_Data->StateId == TSL_STATEID_DETECT) ||

(MyTKeys[(NB)].p_Data->StateId == TSL_STATEID_DEB_RELEASE_DETECT) ||

(MyTKeys[(NB)].p_Data->StateId == TSL_STATEID_TOUCH) ||

(MyTKeys[(NB)].p_Data->StateId == TSL_STATEID_DEB_DETECT))

while (1)

{

if (tsl_user_Exec() == TSL_STATUS_OK)

{

ProcessSensors(); // Execute sensors related tasks

}

}

void ProcessSensors (void)

{

if (TEST_TKEY(0))

{

HAL_GPIO_WritePin(LD4_GPIO_Port, LD3_Pin, GPIO_PIN_SET);

}

else

{

HAL_GPIO_WritePin(LD4_GPIO_Port, LD3_Pin, GPIO_PIN_RESET);

}

if (TEST_TKEY(1))

{

HAL_GPIO_WritePin(LD4_GPIO_Port, LD4_Pin, GPIO_PIN_SET);

}

else

{

HAL_GPIO_WritePin(LD4_GPIO_Port, LD4_Pin, GPIO_PIN_RESET);

}

if (TEST_TKEY(2))

{

HAL_GPIO_WritePin(LD4_GPIO_Port, LD5_Pin, GPIO_PIN_SET);

}

else

{

HAL_GPIO_WritePin(LD4_GPIO_Port, LD5_Pin, GPIO_PIN_RESET);

}

}

static void MX_TSC_Init(void)

{

/** Configure the TSC peripheral

htsc.Instance = TSC;

htsc.Init.CTPulseHighLength = TSC_CTPH_2CYCLES;

htsc.Init.CTPulseLowLength = TSC_CTPL_2CYCLES;

htsc.Init.SpreadSpectrum = DISABLE;

htsc.Init.SpreadSpectrumDeviation = 1;

htsc.Init.SpreadSpectrumPrescaler = TSC_SS_PRESC_DIV1;

htsc.Init.PulseGeneratorPrescaler = TSC_PG_PRESC_DIV4;

htsc.Init.MaxCountValue = TSC_MCV_8191;

htsc.Init.IODefaultMode = TSC_IODEF_OUT_PP_LOW;

htsc.Init.SynchroPinPolarity = TSC_SYNC_POLARITY_FALLING;

htsc.Init.AcquisitionMode = TSC_ACQ_MODE_NORMAL;

htsc.Init.MaxCountInterrupt = DISABLE;

htsc.Init.ChannelIOs = TSC_GROUP1_IO3|TSC_GROUP2_IO3|TSC_GROUP3_IO2;

htsc.Init.ShieldIOs = 0;

htsc.Init.SamplingIOs = TSC_GROUP1_IO4|TSC_GROUP2_IO4|TSC_GROUP3_IO3;

if (HAL_TSC_Init(&htsc) != HAL_OK)

{

Error_Handler();

}

}

I don't understand what is it that I am doing wrong and how can I configure 3 touch keys on this slider with adjustable detect threshold?

Your support with these questions is much appreciated and would be very helpful for me to understand and learn TSC and Touch application..

Thank you.

This topic has been closed for replies.
OlivierR
OlivierRBest answer
ST Employee
Aug 18, 2020 12:41 PM UTC

Hello,

Find attached a TSC project:

  • DISCO-F072B
  • Slider 3 channel half-ended
  • TSC Interrupt management
  • Resolution = 7 , mean Position will move from 1 to 127
  • Generate using ioc STM32CubeMx file
  • IAR ide

I hope it will help.

Olivier

2 replies

OlivierR
OlivierRBest answer
ST Employee
Aug 18, 2020 12:41 PM UTC

Hello,

Find attached a TSC project:

  • DISCO-F072B
  • Slider 3 channel half-ended
  • TSC Interrupt management
  • Resolution = 7 , mean Position will move from 1 to 127
  • Generate using ioc STM32CubeMx file
  • IAR ide

I hope it will help.

Olivier

MS.1134
MS.1134Author
Associate II
Aug 18, 2020 1:23 PM UTC

thank you so much, OlivierR

I will review the attached project and will work on my practice project again accordingly to fully understand the concept.

I will let you know if I run into any further questions.