Skip to main content
DPark.2
Associate III
August 14, 2020
Solved

have problem on get internal temperature sensor value in STM32F091

When getting the value from the internal temperature sensor, the value is not stable.

I am testing it inside the office, and the chip surface temperature is 25 degrees Celsius.

The code outputs the internal temperature sensor value every second, and it is output as follows.

​

temp 334

temp 333

temp 334

​temp 334

temp 334

temp 68

temp 333

temp 68

temp 68

temp 333

temp 333

temp 334

temp 68

temp 68

temp 68

temp 334

temp 334

temp 68

temp 334

​

​I'm not sure if the init code or import code is wrong.

​

```C

// ADc Init Code

static void MX_ADC_Init(void)

{

  /* USER CODE BEGIN ADC_Init 0 */

  ADC1->CHSELR = ADC_CHSELR_CHSEL16;                              /* (1) */

  ADC1->SMPR |= ADC_SMPR_SMP_0 | ADC_SMPR_SMP_1 | ADC_SMPR_SMP_2; /* (2) */

  ADC->CCR |= ADC_CCR_TSEN;                                       /* (3) */

  /* USER CODE END ADC_Init 0 */

  ADC_ChannelConfTypeDef sConfig = {0};

  /* USER CODE BEGIN ADC_Init 1 */

  /* USER CODE END ADC_Init 1 */

  /** Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion) 

  */

  hadc.Instance = ADC1;

  hadc.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;

  hadc.Init.Resolution = ADC_RESOLUTION_12B;

  hadc.Init.DataAlign = ADC_DATAALIGN_RIGHT;

  hadc.Init.ScanConvMode = ADC_SCAN_DIRECTION_FORWARD;

  hadc.Init.EOCSelection = ADC_EOC_SINGLE_CONV;

  hadc.Init.LowPowerAutoWait = DISABLE;

  hadc.Init.LowPowerAutoPowerOff = DISABLE;

  hadc.Init.ContinuousConvMode = ENABLE;

  hadc.Init.DiscontinuousConvMode = DISABLE;

  hadc.Init.ExternalTrigConv = ADC_SOFTWARE_START;

  hadc.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;

  hadc.Init.DMAContinuousRequests = DISABLE;

  hadc.Init.Overrun = ADC_OVR_DATA_PRESERVED;

  if (HAL_ADC_Init(&hadc) != HAL_OK)

  {

    Error_Handler();

  }

  /** Configure for the selected ADC regular channel to be converted. 

  */

  sConfig.Channel = ADC_CHANNEL_2;

  sConfig.Rank = ADC_RANK_CHANNEL_NUMBER;

  sConfig.SamplingTime = ADC_SAMPLETIME_239CYCLES_5;

  if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)

  {

    Error_Handler();

  }

  /** Configure for the selected ADC regular channel to be converted. 

  */

  sConfig.Channel = ADC_CHANNEL_TEMPSENSOR;

  if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)

  {

    Error_Handler();

  }

  /* USER CODE BEGIN ADC_Init 2 */

  /* USER CODE END ADC_Init 2 */

}

```

​

```C

// print ADC Temp Code

void printTemp(void)

{

  // ADC1->CR |= ADC_CR_ADSTART;

  // while ((ADC1->ISR & ADC_ISR_EOC) == 0)

  // {

  // };

  int32_t temperature; /* will contain the temperature in degrees Celsius */

  temperature = (((int32_t)ADC1->DR * VDD_APPLI / VDD_CALIB) - (int32_t)*TEMP30_CAL_ADDR);

  temperature = temperature * (int32_t)(110 - 30);

  temperature = temperature / (int32_t)(*TEMP110_CAL_ADDR - *TEMP30_CAL_ADDR);

  temperature = temperature + 30;

  DEBUG_PRINT_RN("temp %d\r\n", (int32_t)temperature);

}

```

​

Reference link

This topic has been closed for replies.
TDK
TDKBest answer
August 14, 2020

I would guess you're converting both channel 2 and the temp sensor. That's what it looks like your initialization code does.

"If you feel a post has answered your question, please click ""Accept as Solution""."

3 replies

waclawek.jan
Super User
August 14, 2020

Prepare and post a minimal but complete compilable code exhibiting the problem.

JW

DPark.2
DPark.2Author
Associate III
August 14, 2020

I posted only the ADC related initialization code and the code of the function to get the temperature.

Is it said that there are more than necessary? Conversely, is it saying that there is no necessary part?

TDK
TDKBest answer
August 14, 2020

I would guess you're converting both channel 2 and the temp sensor. That's what it looks like your initialization code does.

"If you feel a post has answered your question, please click ""Accept as Solution""."