HAL I2C always sends 0xFF as first byte when responding to master using HAL_I2C_Slave_Transmit
I have an STM32G4 using the HAL function HAL_I2C_Slave_Transmit to respond with some data when requested by a master on the I2C bus. In the image below you can see the device sends 0xFF followed by the actual data it was meant to send (the data I am expecting is 0x11 0x01 0x00).

If I instead use HAL_I2C_Slave_Transmit_IT then I get a worse result, as shown below:

I have tried this with the minimal test program below so I don't believe it's anything to do with my full program having a delay:
/* USER CODE BEGIN 2 */
typedef struct {
char id;
char payload[2];
} I2C_RSP_TO_MASTER;
I2C_RSP_TO_MASTER I2C_response;
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
I2C_response.id = 0x11;
I2C_response.payload[0] = 0x01;
I2C_response.payload[1] = 0x00;
HAL_I2C_Slave_Transmit(&hi2c2, (uint8_t*) &I2C_response, 3, 10);
while (HAL_I2C_GetState(&hi2c2) != HAL_I2C_STATE_READY) {
}
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */For my current testing the master is an Arduino Nano using the Arduino function:
Wire.requestFrom(ADDR, 4);I am requesting 4 bytes because the initial byte is garbage (0xFF). The STM32 is clocked at 128MHz so I don't believe it is possible that it is running too slowly to respond to the first byte - I think it must be a problem with the HAL! Any advice?