Question
Is there a way to power a nucleo 64 board from a 3V external battery without damaging the board?
Hello,
I'd like to power my nucleo L152RE from a 3V external battery.
I thought this should be easy but then I read that some soldering needed to be done? Is that true? I'd like to be able to power the board from an external 3V battery to use it as an autonomous device, then reconnect it to the PC via USB when updating my program, or just experimenting with new programs.
Is there a way to power the nucleo from an external 3V battery without soldering or unsoldering stuff?
Thanks for your help.