Skip to main content
BCora.1
Associate III
August 9, 2020
Question

How to launch openocd for the nucleo stm32l152?

  • August 9, 2020
  • 4 replies
  • 3681 views

Hello,

I'm new to embedded programming and to the stm32 platform.

I'm using linux. I need to debug and inspect the memory of the device. Openocd seems to be the preferred (perhaps the only way?) to do this on linux. I installed openocd but despite long searches on the internet, it's not clear how to launch it to work with my nucleo L152RE.

When I run

openocd

on the command line, I get

Open On-Chip Debugger 0.10.0
Licensed under GNU GPL v2
For bug reports, read
	http://openocd.org/doc/doxygen/bugs.html
embedded:startup.tcl:60: Error: Can't find openocd.cfg
in procedure 'script' 
at file "embedded:startup.tcl", line 60
Error: Debug Adapter has to be specified, see "interface" command
embedded:startup.tcl:60: Error: 
in procedure 'script' 
at file "embedded:startup.tcl", line 60

How can I run the program?

Thanks for your help.

Thanks for your help.

This topic has been closed for replies.

4 replies

TDK
August 9, 2020

As the error message states, OpenOCD needs a configuration file. There should be a number of them in the openocd driectory, probably one that matches up with your L153 board.

http://openocd.org/doc/html/Running.html

"If you feel a post has answered your question, please click ""Accept as Solution""."
BCora.1
BCora.1Author
Associate III
August 9, 2020

I can't seem to find config files that would match my device.

$ find /usr/share/openocd/ | grep interface | grep stm32

returns:

/usr/share/openocd/scripts/interface/ftdi/stm32-stick.cfg

And:

$ find /usr/share/openocd/ | grep board | grep stm32l

returns:

/usr/share/openocd/scripts/board/stm32ldiscovery.cfg
/usr/share/openocd/scripts/board/stm32l4discovery.cfg
/usr/share/openocd/scripts/board/stm32l0discovery.cfg

However, when I do:

$ find /usr/share/openocd/scripts/ | grep stm32l

I get:

/usr/share/openocd/scripts/target/stm32l0.cfg
/usr/share/openocd/scripts/target/stm32l1.cfg
/usr/share/openocd/scripts/target/stm32l4x.cfg
/usr/share/openocd/scripts/target/stm32l1x_dual_bank.cfg
/usr/share/openocd/scripts/target/stm32lx_stlink.cfg
/usr/share/openocd/scripts/board/stm32ldiscovery.cfg
/usr/share/openocd/scripts/board/stm32l4discovery.cfg
/usr/share/openocd/scripts/board/stm32l0discovery.cfg

Maybe the /usr/share/openocd/scripts/target/stm32l1x_dual_bank.cfg would correspond to my device but if I use this file like this:

$ openocd -f /usr/share/openocd/scripts/target/stm32l1x_dual_bank.cfg

I get an error:

Open On-Chip Debugger 0.10.0
Licensed under GNU GPL v2
For bug reports, read
	http://openocd.org/doc/doxygen/bugs.html
Error: Debug adapter does not support any transports? Check config file order.
Error: unable to select a session transport. Can't continue.
shutdown command invoked

TDK
August 9, 2020
The config file you want is in the board directory.
Instead of guessing at the naming convention, open the directory and look through. The naming convention is anything but standardized.
"If you feel a post has answered your question, please click ""Accept as Solution""."
BCora.1
BCora.1Author
Associate III
August 9, 2020

Thank you! There's indeed a st_nucleo_l1.cfg file in the /usr/share/openocd/scripts/board/ directory. I guess that must be it.

I tried:

$ openocd -f /usr/share/openocd/scripts/board/st_nucleo_l1.cfg

and I got no error message so I guess it must be working. I have to try some debugging or read some memory from the device to be sure.

I'm pretty optimistic despite apparently a few warnings:

Open On-Chip Debugger 0.10.0
Licensed under GNU GPL v2
For bug reports, read
	http://openocd.org/doc/doxygen/bugs.html
adapter speed: 300 kHz
adapter_nsrst_delay: 100
Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD
none separate
srst_only separate srst_nogate srst_open_drain connect_deassert_srst
Info : Unable to match requested speed 300 kHz, using 240 kHz
Info : Unable to match requested speed 300 kHz, using 240 kHz
Info : clock speed 240 kHz
Info : STLINK v2 JTAG v30 API v2 SWIM v19 VID 0x0483 PID 0x374B
Info : using stlink api v2
Info : Target voltage: 3.262426
Info : stm32l1.cpu: hardware has 6 breakpoints, 4 watchpoints