Skip to main content
GZeyf.1
Associate
Aug 6, 2020 6:04 PM UTC
Question

After the last update STM32CubeIDE to 1.4.1 the SD card stopped working on STM32F4...

The bundle FreeRtos+ FATfs stopped working. In version embedded software 1.25.0 and 1.24.. When I trying to call f_mount() the system freezes completely. I took two days to find the problem! In file sd_diskio.c (FATfs) queue function is called (osMessageQueuePut) from the interrupt. This leads to a complete system crash. Even I, after two weeks of studying STM, know that you cannot call a queue from an interrupt! 

I had to replace the sd_diskio.h and sd_diskio.c files with files from version 1.23. There, instead of a queue, the usual flag is applied. After that, everything worked. But the files are replaced after each generation with a cube. 

Questions:

Is it generally normal that after the next updates everything collapses due to children's mistakes?

How can I manually select in a cube not the latest version of embedded software? This tab is there but it is not active despite the fact that many versions have been downloaded.

0693W000003OfAgQAK.jpg0693W000003Of9xQAC.jpg

This topic has been closed for replies.

1 reply

S.Ma
Principal
Aug 6, 2020 7:59 PM UTC

Upgrading tool while a project has already started creates additional setbacks risks. Can you afford it? It is worth it?