cancel
Showing results for 
Search instead for 
Did you mean: 

Can unpowered H7 MCU suffer active IO?

JZou.2
Associate II

The H7 MCU may be powered off by ex controller. At this suitation, can this unpowered MCU suffer other active IOs?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
waclawek.jan
Super User

This depends on particular pins. 5V tolerant pins (marked FT and similarly, in the pin table in Datasheet) are usually specified to VDD+4.0V, i.e. they should be able to withstand 3V signals even when VDD=0V. Non-5V-tolerant pins (marked TT and similarly) usually can't go above VDD. Read the IO-relevant portions of the Operating conditions chapter in Datasheet.

JW

0693W000002lUOZQA2.png

On this table, I can see tha max input for FT and TT are not less than 4.0V. Is this 4.0V still avaliable even VDD = 0v(mcu powered off)?