Question
Has anybody already tried the new CubeIDE 1.4.1 and Touch GFX 4.14, I cannot get it working.
I did start the project with F469I Discovery board, I got all the settings then I add Graphics Application it generates new folder TouchGFX.
I start from this folder TouchGFX, I build simple screen, generate code.
then I build the projects no errors I upload to the board.
dark screen, nothing there.
am I missing something ?
I got all the same setting for LTDC like RGB888, 800 x 480 pixels form other working project I ma sure I am not missing anything here
how do I set it up so it works ?