Skip to main content
egoltzman
Senior
July 29, 2020
Solved

After porting from 1.3.1 to 1.4 all NVIC priorities changed to 0 while FreeRTOS MAX Int Priority allow not less then 5

I have a running project that is based on CubeIDE 1.3.1 and it includes FreeRTOS, FATFS, USB_Device and TouchGFX running on F429.

After upgrade to 1.4 and regenerate the code based on the project existing IOC I saw that all the interrupt priorities changed from 5 to 0 and the system stopped working. Only after I changed it manually to 5 it started to work again.

FreeRTOS is defined with:

#define configLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITY 5

In the previous CubeIDE version the generated code made the NVIC IRQ interrupt to be depend on that value and all the default IRQ priorities was 5.

Any input on that?

This topic has been closed for replies.
Nesrine.JLASSI
Nesrine.JLASSIBest answer
Visitor II
July 30, 2020

Hello,

A new STM32CubeMX release will delivered to correct this issue as soon as possible.

Best regards,

Nesrine

5 replies

Nesrine.JLASSI
Visitor II
July 29, 2020

Hello @egoltzman​ 

Could you please share your project to check the issue.

Best regards,

Nesrine

Nesrine.JLASSI
Visitor II
July 30, 2020

Hello @egoltzman​ 

Thanks for the feedback, issue reported to the tool development team that will plan the correction.

Best regards,

Nesrine

Nesrine.JLASSI
Nesrine.JLASSIBest answer
Visitor II
July 30, 2020

Hello,

A new STM32CubeMX release will delivered to correct this issue as soon as possible.

Best regards,

Nesrine

S.Ma
Principal
August 6, 2020

Has it been thoroughly tested to make sure there is no side effect or collateral damage? There seems to be fresh posts about user project folders deleted, fixed and not fully fixed post today...