QUAD SPI read not working
- July 29, 2020
- 3 replies
- 2198 views
Hi all,
I am working with STM32L476RG and using ST32cubeIDE for developing project. I am trying to enable Quad SPI in my project . I am using MX25R8035FM1IL0 as flash memory. I followed the code in the software package of ST, but it is not working.
When i am reading from reception buffer i am receiving nothing.
my Quad SPI configurations;
- prescalar -2
- flash size -14
- fifothreshold- 4
i am using instruction , address and data on a single line. when i tried address and data modes with 4 lines, in the reception buffer i am getting value 136 in decimal
Rx and Tx callback are coming when i checked with break points.
I am unable to find the issue in my code .
can anybody help me?
This is the Reference code i used from ST: STM32Cube_FW_L4_V1.15.0\Projects\STM32L476G-EVAL\Examples\QSPI\QSPI_ReadWrite_IT