Skip to main content
Alihussain Vohra
Associate III
July 25, 2020
Question

IAP UART is not working

  • July 25, 2020
  • 5 replies
  • 2012 views

I am using stm32f072 discover board. I am developing IAP UART code. I take the reference code provided in the repository. I am attaching the code too. I am also following application note AN4065 and AN4657. The option for downloading and uploading, executing is coming on terminal. When I try to transmit the file then it is hangs on the wait. Thanks in advance for the help.

This topic has been closed for replies.

5 replies

Tesla DeLorean
Guru
July 25, 2020

ZIP up the project rather than attach half a dozen files.

Identify your code/additions.

Try debugging, or identifying actual failure. Saying it hangs is of little help. Stop in the debug and inspect where it is stuck. Waiting on characters, getting what it needs? Stuck in a while(1) loop.

Try different terminal applications.

Show interaction.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Alihussain Vohra
Associate III
July 27, 2020

I am attaching the zip file of project...The failure is that it points the memory address out of the region...I tried with 2 different terminals but it didn't work

prain
Visitor II
July 27, 2020

Personally I used this example (ymodem) but unfortunately it is not reliable. Forget ymodem and go for newer FTP protocol

Alihussain Vohra
Associate III
July 27, 2020

Can you brief about it?

prain
Visitor II
July 28, 2020

for a light weight and straight forward implementation, take a look on MAVLink FTP protocol​