Skip to main content
Skada.3
Associate III
July 23, 2020
Question

MTU extension leads to HardFault error.

Hi

I am using Bluenrg_m2 expansion board X_Nucleo_Bluenrg2 along with the controller Stm32l476rg. Reffered example is 'SampleApp' form X_cuble_BLE2_v1.0.0.

I am trying to send 160 bytes of the fixed data over BLE frequently but after sending one packet of the data I am getting Hard_fault_error exception.

I tried to increase the heap size and stack size as well.

Also change the HCI_MAX_PAYLOAD_SIZE from 128 to 256 (not sure, this change is needed or not)

Not able to get the hard fault issue, looking for the solution on this issue.

This topic has been closed for replies.