Skip to main content
HGüne.1
Associate
July 23, 2020
Solved

STGAP1AS mosfet driver paralleled mosfets active miller clamp.

  • July 23, 2020
  • 4 replies
  • 1402 views

Hello.

How can i use active miller clamp function of STGAP1AS mosfet driver for paralleled mosfets?

This topic has been closed for replies.
Best answer by Cristiana SCARAMEL

Hello @Hilmi Güney​ ,

I edited my previous post because I forgot the picture :grinning_face_with_sweat:

I suggest to modify the gate resistors connection to reduce the current unbalance (see picture below).

Any variation, not so much of resistance value, but of gate paths (parasitic inductance and resistance of the traces) will affect current balance.

Each gate path trace must be kept as short as possible, moreover a symmetrical length traces are suggested.

With this configuration you can use two different gate resistors for turn and turn off.

0693W000003BKtjQAG.png

4 replies

Cristiana SCARAMEL
ST Employee
July 24, 2020

Hello @Hilmi Güney​ welcome to the ST Community.

You can use the Miller Clamp function connecting the CLAMP pin to the connection point of the MOSFETs gate (refer to below picture).

The CLAMP pin monitors the voltage at the gate connection when the MOSFET is off.

The internal CLAMP switch is activated when the voltage goes below the voltage threshold VCLAMPth, thus creating a low impedance path between the MOSFETs gate and the VL pin.

0693W000003BJyOQAW.png

"If you feel a post has answered your question, please click ""Accept as Solution"""
HGüne.1
HGüne.1Author
Associate
July 24, 2020

0693W000003BGihQAG.pngHello @Cristiana SCARAMEL​ 

I am wondering how can i use active miller clamp function 2 paralled mosfets?

Cristiana SCARAMEL
ST Employee
July 27, 2020

Hello @Hilmi Güney​ ,

I edited my previous post because I forgot the picture :grinning_face_with_sweat:

I suggest to modify the gate resistors connection to reduce the current unbalance (see picture below).

Any variation, not so much of resistance value, but of gate paths (parasitic inductance and resistance of the traces) will affect current balance.

Each gate path trace must be kept as short as possible, moreover a symmetrical length traces are suggested.

With this configuration you can use two different gate resistors for turn and turn off.

0693W000003BKtjQAG.png

"If you feel a post has answered your question, please click ""Accept as Solution"""
Cristiana SCARAMEL
ST Employee
August 5, 2020

Hello @Hilmi Güney​,

it is more clear to you how to use the active miller clamp function in your application?

If the answer was helpful, please "Select as Best", thank you.

"If you feel a post has answered your question, please click ""Accept as Solution"""