Skip to main content
siva.1
Visitor II
July 22, 2020
Solved

i bought sreval-stwinkt1 eval board plug and play eval board,

  • July 22, 2020
  • 2 replies
  • 834 views

I need an information that where it is placed on the motor?

    This topic has been closed for replies.
    Best answer by Eleon BORLINI

    Hi @siva.1​ , the placement of the STWINKT board could depend on what do you want to detect of the motor. For example, if you want to detect the vibration of the motor, you should screw it on the vibration motor case itself (same reference system) as shown in the picture below:

    0693W000002lBszQAE.png

    If you otherwise want to perform predictive maintenance with the ultrasound microphone, you are not strictly limited to screw the board on the motor, but you can just place it nearby the vibrating object.

    In any case, I suggest you to check the existing online documentation (e.g. https://www.youtube.com/watch?v=J3M0_9EdOqU and https://www.youtube.com/watch?v=eRDRLiI2DyU)

    Regards

    2 replies

    Eleon BORLINI
    Eleon BORLINIBest answer
    ST Employee
    August 26, 2020

    Hi @siva.1​ , the placement of the STWINKT board could depend on what do you want to detect of the motor. For example, if you want to detect the vibration of the motor, you should screw it on the vibration motor case itself (same reference system) as shown in the picture below:

    0693W000002lBszQAE.png

    If you otherwise want to perform predictive maintenance with the ultrasound microphone, you are not strictly limited to screw the board on the motor, but you can just place it nearby the vibrating object.

    In any case, I suggest you to check the existing online documentation (e.g. https://www.youtube.com/watch?v=J3M0_9EdOqU and https://www.youtube.com/watch?v=eRDRLiI2DyU)

    Regards

    Eleon BORLINI
    ST Employee
    September 15, 2020

    Hi @siva.1​ ,

    was this suggestion of any help for you? Or did you find a good way to mount the STWINKT1 on the motor?

    Please note that the vibration sensor is in the middle of the board...

    -Eleon