Skip to main content
moredatalesscenter
Associate III
July 16, 2020
Question

Text area sometimes contains question marks

  • July 16, 2020
  • 4 replies
  • 2000 views

I've created a wildcard in Designer using https://support.touchgfx.com/docs/development/ui-development/touchgfx-engine-features/texts-and-fonts/ and updating it in handleTickEvent() as per https://support.touchgfx.com/docs/tutorials/tutorial-03/.

Occasionally it's displayed with garbage e.g. 42?5?352. It's fine in the buffer. TEXTAREA1_SIZE is 10.

void Screen1View::updateTxt(int value)

{

 Unicode::snprintf(textArea1Buffer, TEXTAREA1_SIZE, "%d", value);

  textArea1.resizeToCurrentTextWithAlignment();

 textArea1.invalidate();

}

The help says "Remember to call myTextArea.invalidate() before resizing myTextArea if you are decreasing the text area size. If not, you will still see part of the old text area, since it is not covered by the new smaller text area.", but the code sample is the other way round. Either way it still displays garbage.

This topic has been closed for replies.

4 replies

AB1.1
Associate
July 17, 2020

Hello

This could happen when you didn`t specify Wildcard characters/ranges in Text/Typographies window in designer. Missing characters replaced by ? by default

Martin KJELDSEN
Principal III
July 17, 2020

@AB1.1​ is right. Which glyphs were you expecting instead of ? Check your wildcard range and whether or not it covers those unicodes that are displayed as ?.

/Martin

moredatalesscenter
Associate III
July 27, 2020

I see. Would it be possible to add a note about the wildcard range to https://support.touchgfx.com/docs/development/ui-development/touchgfx-engine-features/texts-and-fonts/ or a reference to https://support.touchgfx.com/docs/development/ui-development/designer-user-guide/texts-view/? Similarly a note about snprintfFloat() being needed instead for floats.

Is there any support for displaying enumerated text e.g. Dog, Cat? Is this supported, or simply wildcard range of "A-z"?

moredatalesscenter
Associate III
July 30, 2020

 @Alexandre RENOUX (ST Employee) please see request above