Skip to main content
DWest.1
Associate
July 15, 2020
Solved

ST-LINK not listed Device Manager

  • July 15, 2020
  • 2 replies
  • 1400 views

I have a NUCELO-L433RC-P dev board that was working fine for several days but is no longer visible in Win 10 Device Manager. STLinkUpgrade and STM32CubeProgrammer do not find my ST-LINK. STM32CubeIDE gives the error "Error in initializing ST-LINK device. Reason: ST-LINK DLL error."

Connecting the dev board to a second pc, and everything appears normal. I did a full chip erase from STM32CubeProgrammer without issue.

Back on my primary PC, I checked the Win10 Restore Points and found no changes in the past 7 days. I tried multiple cables and multiple USB ports with no change.

When I plug the dev board into my primary PC, the LD1 light slow blinks red. If I unplug and re-plug a few times, I can get LD1 to fast blink red but the ST-LINK never mounts. While plugging/unplugging the USB, Windows10 never makes the "beep boop" sounds that it should when connecting USB devices.

This topic has been closed for replies.
Best answer by TDK

Do other devices work on that port? Did you reboot? Try using a different cable? Try using a different port?

2 replies

TDK
TDKBest answer
July 15, 2020

Do other devices work on that port? Did you reboot? Try using a different cable? Try using a different port?

"If you feel a post has answered your question, please click ""Accept as Solution""."
DWest.1
DWest.1Author
Associate
July 15, 2020

Amazingly enough. A PC restart is exactly what I needed. Thanks.