Skip to main content
ANaga.2
Associate III
July 14, 2020
Question

SBSFU failure during verifying FW SIGNATURE

  • July 14, 2020
  • 2 replies
  • 822 views

Hi,

I could successfully integrate the SBSFU feature to our application. everything goes well until I get a failure after swapping the images.

FW signature is not getting verified and function SE_SP_SMUGGLE is returning SE_ERROR which is causing the error. I guess I have missed some signature somewhere. I could not debug further as SE_SP_SMUGGLE function leads to some low level programming.

Could anyone help me with this.

Thanks,

Ankush

This topic has been closed for replies.

2 replies

Jocelyn RICARD
ST Employee
July 23, 2020

Hello Ankush,

I made the porting from L432 to L452.

It is working fine on my side.

I join the zip file.

I hope this will help solving your issue

Best regards

Jocelyn

ANaga.2
ANaga.2Author
Associate III
July 28, 2020

Hi Jocelyn,

Thank you so much. We successfully integrated the SBSFU features to our project running on L452 :)

Now we are heading to next step of removing y-modem transfer and including BLE transfer !!

Thanks,

Ankush