Skip to main content
BTrem.1
Senior
July 13, 2020
Question

STM32F30x Definition of Timer signals in DMA mode

  • July 13, 2020
  • 1 reply
  • 824 views

I have a basic question on signal definitions used in the Ref Manual. The section on DMA interconnects refers to TIM3_UP, TIM3_UP, etc, and TIM3_Ch3/UP.

First question: What is UP? This is not defined anywhere. Does it mean TIM3 gets updated?

In CubeMX if I setup to use TIM3 Ch3 and Ch4 I can select as dma TIM3_Ch3 but the other choice for Ch4 is TIM3_Ch4/UP. I'm trying to use an external input for TIM3_Ch4 and use COMP4 input for TIM3_Ch3. Is this possible using TIM3?

I was planning on using TIM2_Ch3 and TIM2_Ch4 for this but for other pinout reasons need to change.

It seems like some of the peripheral request signals in Figure 47 RM0316 are not defined very well.

This topic has been closed for replies.

1 reply

waclawek.jan
Super User
July 13, 2020

> What is UP?

The Update event.

The RM explains, what does it mean (basically it's consequence of over/underflow, but there are also other sources to this signal).

> use an external input for TIM3_Ch4 and use COMP4 input for TIM3_Ch3.

Is this possible using TIM3?

I am not quite sure, what's the question here.. If there's a connection from COMP4 to TIM3_CH3, then it can be used for input capture independently from TIM3_CH4. However, you say that DMA shares trigger from Update and TIM3_CH4 (they are essentially OR-ed), so you should probably not use these two at the same time.

> It seems like some of the peripheral request signals in

> Figure 47 RM0316 are not defined very well.

Which signals, namely?

Maybe try to draw some simple diagram explaining what do you intend to achieve.

JW