Skip to main content
Karan 123
Senior
July 11, 2020
Solved

How to Use STM32G0 Power Voltage Detector with STM32CubeIDE??

  • July 11, 2020
  • 1 reply
  • 3458 views

Hi,

I am working on STM32G0 Nucleo Board with STM32 Cube IDE 1.3.0 .

How to Use STM32G0 Power Voltage Detector (Internal ) with STM32CubeIDE ?

I want my MCU should only start when Voltage goes above 2.5V (Say)..0693W000001sh8tQAA.jpg

The above setting nothing generate in .c file for PVD.

I have also checked below example but nothing configured in PWR_PVD.ioc

..\en.stm32cubeg0\STM32Cube_FW_G0_V1.3.0\Projects\NUCLEO-G071RB\Examples\PWR\PWR_PVD

Thanks in advice ..

Any Other option..

--

Karan

This topic has been closed for replies.
Best answer by Khouloud ZEMMELI

Hello @Community member​ 

From CubeMX side, you need to change PVD level, the 2.5 V is present in parameter options.

Regards,

Khouloud

1 reply

Khouloud ZEMMELI
Khouloud ZEMMELIBest answer
ST Employee
November 17, 2020

Hello @Community member​ 

From CubeMX side, you need to change PVD level, the 2.5 V is present in parameter options.

Regards,

Khouloud