Problems booting with U-boot in Ecosystem 2.0 using the trusted bootchain
- 5 replies
- 2548 views
Hi,
we were facing trouble booting the Ecosystem 2.0 with the new U-Boot (v2020.01-stm32mp-r1).
We are using buildroot as the tool to build our distribution. With the Ecosystem 1.2 we could build everything perfectly and the booting was fine too. We used your Github to get the sources for the trusted boot chain (TF-A, OP-TEE, U-Boot, Kernel).
Recently we migrated to the new Ecosystem 2.0. When using the sources from your github directly we encountered two problems:
- The Kernel wasn't able to load. The problem was a wrong .config file. We used your release from the wiki (the archive file with the patches) to reconstruct the .config file from that. With this new .config file it worked, the kernel got loaded. Just want to point out, that using the 'default' .config file from your github didn't work for us in case it is meant to work straight away.
- The other problem we were facing is that the U-Boot did write the environment variables to the MMC (we have a DK2 board so in that case to the SD card). After rebooting the image check of the U-Boot was failing (see attatched log; TF-A checks the U-Boot image). Some time back I read in this forum that you plan to move the U-Boot environment variables to the end of ssbl (https://community.st.com/s/question/0D53W000004HoKgSAK/uboot-environment-configuration). Obviously that is the case now. The only way to avoid failing the second boot was to put the variables in the rootfs again (using U-Boot menuconfig). Using your .config from the archive release didn't do the trick as it did with the kernel.
We are not signing the images for now, so the checksum embedded in the header is the source for the failure of the image check (see log). The STM32 header of course isn't rewritten by U-Boot when it writes the environment variables (and it shouldn't do it of course).
My question is now, if that is some error on our side (maybe some configuration missed)? Is there some fix to get the environments in the ssbl and using the trusted boot chain?
Cheers