Skip to main content
thomas
Visitor II
July 7, 2020
Question

HAL_ADC_Stop_DMA cause error if called when DMA state != HAL_DMA_STATE_BUSY HAL Version: STM32F3 1.11.0

  • July 7, 2020
  • 1 reply
  • 1965 views

Whenever I call HAL_ADC_Stop_DMA before HAL_ADC_Start_DMA and the last DMA transfer was allready finished i got an unresetable error.

--> HAL_ADC_STATE_ERROR_DMA

This is my sequenze:

1:HAL_ADC_Stop_DMA

2:HAL_ADC_Start_DMA

.

.

1:HAL_ADC_Stop_DMA

2:HAL_ADC_Start_DMA

.

.

1:HAL_ADC_Stop_DMA

2:HAL_ADC_Start_DMA

.

.

At the moment I solved this like this:

   if (hadc->DMA_Handle->State == HAL_DMA_STATE_BUSY) {

       (void)HAL_ADC_Stop_DMA(hadc);

   } else {

       (void)HAL_ADC_Stop_IT(hadc);

   }

When the DMA is allready finished I only call "HAL_ADC_Stop_IT" to stop the ADC measurement. Otherwise I call "HAL_ADC_Stop_DMA".

But shouldent it be possible just to call "HAL_ADC_Stop_DMA" regardless the state of the DMA?.

In my opinion the problem is in the file stm32f3xx_hal_adc_ex line 2669 & 2675.

2269:

tmp_hal_status = HAL_DMA_Abort(hadc->DMA_Handle);  

This call returns a HAL_ERROR with a "HAL_DMA_ERROR_NO_XFER" status.

This is ok when there was no transfer active.

2675:

But then here this message is treated as error. And I can not reset this error.

SET_BIT(hadc->State, HAL_ADC_STATE_ERROR_DMA); 

It also changed from the library version 1.10.0 to 1.11.0.

In 1.10.0 it worked because "tmp_hal_status = HAL_DMA_Abort(hadc->DMA_Handle);" did not return any error.

Is this a bug or am I applying it incorrectly

This topic has been closed for replies.

1 reply

Georgy Moshkin
Senior
January 15, 2021

Same problem on STM32H7 when using ADC Interleaved mode + DMA in single shot mode, and calling HAL_ADCEx_MultiModeStop_DMA. I traced it to HAL_DMA_Abort function in stm32h7xx_hal_dma.c starting from line 792:

 if(hdma->State != HAL_DMA_STATE_BUSY)
 {
 hdma->ErrorCode = HAL_DMA_ERROR_NO_XFER;
 
 /* Process Unlocked */
 __HAL_UNLOCK(hdma);
 
 return HAL_ERROR;
 }

Because of HAL_DMA_ERROR_NO_XFER error code HAL_ADC_STATE_ERROR_DMA bit is set. This bit prevents HAL_ADC_ConvHalfCpltCallback from running for if single shot is started again using HAL_ADCEx_MultiModeStart_DMA.

Normal operation returns if this bit is cleared, but I did not check for any additional errors:

HAL_ADCEx_MultiModeStop_DMA(&hadc1);
CLEAR_BIT(hadc1.State, HAL_ADC_STATE_ERROR_DMA);

Check my STM32 Bootloader - flash your STM32 with AES-encrypted binaries right from web browser!