2020-07-06 12:35 PM
I have been using the Starter-Package v1.2.0 with no problem. But I cannot flash the SD Card with the new v2.0.0 Starter-Package. I am using STM32CubeProg v2.2.0 and I keep getting the same errors (using either CLI or GUI):
$ STM32_Programmer_CLI -c port=usb1 -w flashlayout_st-image-weston/trusted/FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsv
-------------------------------------------------------------------
STM32CubeProgrammer v2.2.0
-------------------------------------------------------------------
USB speed : High Speed (480MBit/s)
Manuf. ID : STMicroelectronics
Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
SN : 0019002B3338510939303435
FW version : 0x0110
Device ID : 0x0500
Device name : STM32MPxxx
Device type : MPU
Device CPU : Cortex-A7
Start Embedded Flashing service
Memory Programming ...
Opening and parsing file: tf-a-stm32mp157c-dk2-serialboot.stm32
File : tf-a-stm32mp157c-dk2-serialboot.stm32
Size : 241984 Bytes
Partition ID : 0x01
Download in Progress:
[==================================================] 100%
File download complete
Time elapsed during download operation: 00:00:00.545
RUNNING Program ...
PartID: :0x01
Start operation done successfully at partition 0x01
Flashlayout Programming ...
[==================================================] 100%
Running Flashlayout Partition ...
Flashlayout partition started successfully
Memory Programming ...
Opening and parsing file: u-boot-stm32mp157c-dk2-trusted.stm32
File : u-boot-stm32mp157c-dk2-trusted.stm32
Size : 870684 Bytes
Partition ID : 0x03
Download in Progress:
[==================================================] 100%
File download complete
Time elapsed during download operation: 00:00:00.971
RUNNING Program ...
PartID: :0x03
reconnecting the device ...
USB speed : High Speed (480MBit/s)
Manuf. ID : STMicroelectronics
Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x2000, @Name /STM32MP157CAC Rev.B,
SN : 0019002B3338510939303435
FW version : 0x0110
Device ID : unknown
Start operation done successfully at partition 0x03
Memory Programming ...
Opening and parsing file: tf-a-stm32mp157c-dk2-trusted.stm32
File : tf-a-stm32mp157c-dk2-trusted.stm32
Size : 241984 Bytes
Partition ID : 0x04
Download in Progress:
Error: failed to download Segment[0]
Error: failed to download the File
Time elapsed during download operation: 00:00:30.005
Error: Download partition 0x04 failed
Error: TSV flashing service failedI can still successfully flash the SD Card with the old v1.2.0 package. Any ideas?
Solved! Go to Solution.
2020-07-06 11:47 PM
Hello Diego,
V2.0.0 is only compatible with V2.4.0 Cube programmer at least, you can download it from st.com.
We have seen some issue also with Netac branded sdcard, this can be also checked.
2020-07-06 11:47 PM
Hello Diego,
V2.0.0 is only compatible with V2.4.0 Cube programmer at least, you can download it from st.com.
We have seen some issue also with Netac branded sdcard, this can be also checked.
2020-07-07 7:18 AM
Thank you!