Skip to main content
ledi001
Associate III
July 3, 2020
Question

Debugger connection don't work with ST-Link and STM32CubeIDE V.1.3.1

  • July 3, 2020
  • 1 reply
  • 685 views

I am working with Windows10, STM32CubeIDE V.1.3.1 and ST-Link on board of NUCLEO-L412KB. Today i connected the board first time and made an update after being asked to do so. After reconnecting the board and successfully update of ST-Link the debugger lost it's connection after starting debugging process.

STMicroelectronics ST-LINK GDB server. Version 5.5.0

Copyright (c) 2019, STMicroelectronics. All rights reserved.

Starting server with the following options:

    Persistent Mode      : Disabled

    Logging Level       : 1

    Listen Port Number     : 61234

    Status Refresh Delay    : 15s

    Verbose Mode        : Disabled

    SWD Debug         : Enabled

    InitWhile         : Enabled

Waiting for debugger connection...

Debugger connected

Debugger connection lost.

Shutting down...

After that, the Debugger LED on NUCLEO board remains red until i restart my PC. After restart, the LED lights up green, but after starting debugging process all is the same behavior like before.

Please help!

This topic has been closed for replies.

1 reply

Jorge Jacome
Associate
July 10, 2020

Something similar did happen to me .

I do pinpoint ,after it does the St-link upgrade cause that problem, in the future I will not do the upgrade until STM fix bugs.

Anyway the way how I did overcome this problem; after following instructions from another St community member.

Delete all projects currently on your workbench, and start a fresh project from scratch .

And its working on Windows 7,8 and 10

Hopefully fix and good luck

Jorge