Skip to main content
MLemo.1
Associate III
June 27, 2020
Question

Unable to program a Disco board with STM32CubeIDE st-link not found

  • June 27, 2020
  • 4 replies
  • 2106 views

Hi,

I'm trying to program my 32L0538DISCOVERY board using the STM32CubeIDE but after trying to upload to it it says that:

 0693W000001reSFQAY.png

and offers me to update the st link firmware with st link upgrade so it fin'd it there and everything but when I hit the "Open in update mode" it seems to disconnect the usb port and nothing happens afterwards...

Any idea how to fix that?

This topic has been closed for replies.

4 replies

MLemo.1
MLemo.1Author
Associate III
June 27, 2020

Also can't Upgrade my ST link V2 programmer saying it doesn't find it but it does appear under device manager under USB (But not COM port)

mattias norlander
ST Employee
June 30, 2020

Un-plug and re-plug the board as indicated in the screenshot above. This is required on some boards, on some boards it is enough to just click open in update mode.

MLemo.1
MLemo.1Author
Associate III
July 12, 2020

Yeah so apperantly nothing makes it work and when opening in update mode is simply disconnect the port and shows as error.

MLemo.1
MLemo.1Author
Associate III
July 9, 2020

Apperantly that's a driver issue...