Skip to main content
Mark81
Associate III
June 25, 2020
Question

What are the "STM32-based control board"?

In the manual of STEVAL-IPM08B I read:

"The STEVAL-IPM08B is compatible with ST's STM32-based control board, enabling designers to build a complete platform for motor control."

I wonder what are these "STM32-based control board" that are compatible with the signal connector.

By the way, in the same document I read:

"Motor control connector (32 pins) interfacing with ST MCU boards"

but in the schematic that connector has 34 pins....

This topic has been closed for replies.

4 replies

KnarfB
Super User
June 27, 2020

There are many choices for a control board from the Nucleo and Eval serieses. You may install the ST Motor Control Workbench and when you start a new project you see dropdown lists for control and power boards.

hth

KnarfB

Mark81
Mark81Author
Associate III
June 28, 2020

Well, few odd things. I'm not talking to you directly (instead I thank you a lot for your answer!) but to any ST's employer:

  • as far as I understand there are not so many choices for a control board compatible with the 34-pins connector. It seems there are only two: STM3210B-EVAL and another one but both of them are obsolete. Of course I can use any other suitable dev-board making the connection wire-by-wire - which is ok - but you cannot say they are compatible with that connector.
  • the ST Motor Control Workbench seems to be available for Windows only!!! How is it possible? I don't use Windows so I cannot use this tool? I can understand if a manufacturer releases its tools for Windows only. One can just avoid it and select a different brand. But when a manufacturer (like ST) releases some tools for Linux (or other OS) and some for Windows only it's very confusing and unfair.

Claire O.
ST Employee
June 30, 2020

Dear Mark81,

we are also unhappy about windows only limitation and preparing a new tools generation to palliate to this problem. It should arrive later this year...

Thanks for your patience,

Claire

KnarfB
Super User
June 29, 2020

Hi Mark81,

I don't have tested it, but there is an adapter board https://www.st.com/en/ecosystems/x-nucleo-ihm09m1.html