Question
Timer synchronization maximum frequency
Hi,
If I am starting with 120 MHz system clock and want the master timer to generate a 60 MHz PWM waveform and I want the second timer to generate an in-phase 8 MHz PWM waveform I must clock the second timer with 120 MHz (as 60 MHz isn't divisible by 8). Can this be achieved by configuring the first timer to generate TRGO from ENABLE and configuring the second timer in GATED_MODE from TRGI? (Or is this self-evident?)
Best regards
Niclas