Skip to main content
BRaj_48
Associate II
June 21, 2020
Question

Does LSM303 has high sensing range than the bosch BMM150 sensor in terms of magnetic field range(x,y,z)(micro tesla)?

  • June 21, 2020
  • 3 replies
  • 1590 views

Have been working with magnetometers for the car parking application. the previous sensors used has not satisfied the range for the application required. Does LSM303 detect at a range of 30cms?

    This topic has been closed for replies.

    3 replies

    Eleon BORLINI
    ST Employee
    June 22, 2020

    Hi @BRaj_48​ , as I can see from the BMM150 sensor datasheet, the magnetometer dynamic range is ±13 gauss on x and y axis and ±25 gauss along z axis, while the sensitivity is 3 mgauss/LSB. On the other hand, the LSM303AGR magnetometer part has a wider dynamic range (±50 gauss), while the minimum detectable signal is 1.5mgauss. The LSM303AGR capability is higher both in terms of Full Scale and resolution, so I believe that it can be cover your application requirements. Regards

    BRaj_48
    BRaj_48Author
    Associate II
    June 23, 2020

    Thank you for your time @Eleon BORLINI​, and i have an another doubt as which will have the capability to detect maximum distance is it milli-tesla or the micro-tesla(as the dynamic range)?

    Eleon BORLINI
    ST Employee
    June 25, 2020

    Should be some tenth of mT... Regards