Skip to main content
SS.5
Associate
June 19, 2020
Question

Can we do XiP with STM32L476RE? Will the performance be good with running code from external memory?

  • June 19, 2020
  • 2 replies
  • 901 views

Hello,

I am using STM32L476RE and want to do XiP. So will it support XiP?

Will the performance be good with running code from external memory?

TIA

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
June 19, 2020

I believe it supports QSPI, other L4's do. Would take a couple of hours of engineering time to test specifics.

Sorry not benchmarked it, but several L4 DISCO/EVAL boards with QSPI that you could test with.

The CM4 doesn't having caching, so external memory is definitely slower, perhaps 2x or 3x, depend on memory and settings. The Micron parts support DDR.

Performance will be adequate, put high stress code in internal RAM/FLASH

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
SS.5
SS.5Author
Associate
June 19, 2020

Thank you