Skip to main content
ICohe.1
Associate III
June 17, 2020
Question

PVD code not generated by CubeIDE (but do in CubeMX)

  • June 17, 2020
  • 2 replies
  • 1271 views

Trying to to use PVD on F401 and CubeIDE but no relevant code is generated.

I found on this forum code generated by CubeMx and it also works for me. Just copy and paste and corrected some minor differences like PVD_AVD_IRQn should be PVD_IRQn

So my question is: How do I make CubeIDE generating code for activating PVD ?

The only relevant Item I found in CubeIDE is PVD interrupt through EXTI line 16

Here is what CubeMX generated:

The following code was generated by CubeMX in stm32h7xx_hal_msp.c:

void HAL_MspInit(void)
{
 /* USER CODE BEGIN MspInit 0 */
 
 /* USER CODE END MspInit 0 */
 PWR_PVDTypeDef sConfigPVD = {0};
 
 __HAL_RCC_SYSCFG_CLK_ENABLE();
 
 /* System interrupt init*/
 /* PendSV_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(PendSV_IRQn, 15, 0);
 
 /* Peripheral interrupt init */
 /* PVD_AVD_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(PVD_AVD_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(PVD_AVD_IRQn);
 
 /** PVD Configuration 
 */
 sConfigPVD.PVDLevel = PWR_PVDLEVEL_7;
 sConfigPVD.Mode = PWR_PVD_MODE_IT_RISING;
 HAL_PWR_ConfigPVD(&sConfigPVD);
 /** Enable the PVD Output 
 */
 HAL_PWR_EnablePVD();
 
 /* USER CODE BEGIN MspInit 1 */
 
 /* USER CODE END MspInit 1 */
}

To those which are totally clueless (like me) you have also to create the following function that will be called when PVD is activated:

void HAL_PWR_PVDCallback(void)

This topic has been closed for replies.

2 replies

Nesrine.JLASSI
Visitor II
October 26, 2020

Hello @ICohe.1​ 

Could you please share your ioc file to check with.

Best regards,

Nesrine

ICohe.1
ICohe.1Author
Associate III
October 26, 2020

Attached is my ioc file as it is now. in CubeIDE 1.4.2

It is possible that at the time of my original post, I used another version.

It is 4 month ago and the project is running because I found a solution as I wrote. I haven't tested if the issue was corrected in the current version.

Anyway thanks for getting back to me and I hope others will benefit from it.