Skip to main content
Eremizin
Associate II
June 17, 2020
Question

Where I can find the example of usbpd_dpm_user.h ?

  • June 17, 2020
  • 3 replies
  • 2339 views

Hello!

I am tryig to create my own USBPD project on P-NUCLEO-USB002, and using UM2552 manual.

I add to project some files (see screenshot) 0693W000001qusqQAA.jpgand have compile error.

On the page 20 there is string: "For details see the file usbpd_dpm_user.h, which contains the structure definition for USBPD_HandleTypeDef." And the thing is that there is no such file in X-CUBE-USBPD STM32_USBPD_Library files. Only in Projects\STM32F072RB-Nucleo\Applications\USB_PD\EVAL_FUSB307_DRP\Src I can find it, but I dont think, that it is correct to use it in my project.

This topic has been closed for replies.

3 replies

Yohann M.
ST Employee
June 18, 2020
Eremizin
EremizinAuthor
Associate II
June 18, 2020

Hello, @Yohann M.​ .

Thank you for answer!

Ok, G0/L5/L4 this models have UCPD on the board.

But if want to use x-code-usbpd with F0?

There is (https://github.com/STMicroelectronics/STM32CubeF0/tree/master/Projects) no examples for usb power delivery, looks like.

I just little understand, how I have to create this files?

Because STM32CubeMX generate it when I am using G0 series controller, but it is have different name.

But when I trying to use library after read the user manual um2552 there is no enouth info to create project.

I understand that it is complex and difficult project, and I understand that I have to read alot of info, but what I have to read?)

Even in USB-PD Core Stack User Maual this files are not included and looks like this files I have to write by myself, but how to do it correct?

Yohann M.
ST Employee
June 19, 2020

Hello,

DPM user code is a common code between all the platforms. You may use G0/L5/G4 code as example and use it for your F0 applications.

In the X-CUBE-USBPD, you will have the same files as well:

(.\Firmware\Projects\STM32F072RB-Nucleo\Applications\USB_PD\EVAL_FUSB307_DRP\Inc\usbpd_dpm_user.h)
 
/**
 * @brief USBPD DPM handle Structure definition
 * @{
 */
typedef struct
{
 uint32_t DPM_ListOfRcvSRCPDO[USBPD_MAX_NB_PDO]; /*!< The list of received Source Power Data Objects from Port partner
 (when Port partner is a Source or a DRP port). */
 uint32_t DPM_NumberOfRcvSRCPDO; /*!< The number of received Source Power Data Objects from port Partner
 (when Port partner is a Source or a DRP port).
 This parameter must be set to a value lower than USBPD_MAX_NB_PDO */
 uint32_t DPM_ListOfRcvSNKPDO[USBPD_MAX_NB_PDO]; /*!< The list of received Sink Power Data Objects from Port partner
 (when Port partner is a Sink or a DRP port). */
 uint32_t DPM_NumberOfRcvSNKPDO; /*!< The number of received Sink Power Data Objects from port Partner
 (when Port partner is a Sink or a DRP port).
 This parameter must be set to a value lower than USBPD_MAX_NB_PDO */
 uint32_t DPM_RDOPosition; /*!< RDO Position of requested DO in Source list of capabilities */
 uint32_t DPM_RequestedVoltage; /*!< Value of requested voltage */
 uint32_t DPM_RequestedCurrent; /*!< Value of requested current */
 int16_t DPM_MeasuredCurrent; /*!< Value of measured current */
 uint32_t DPM_RDOPositionPrevious; /*!< RDO Position of previous requested DO in Source list of capabilities */
 uint32_t DPM_RequestDOMsg; /*!< Request Power Data Object message to be sent */
 uint32_t DPM_RequestDOMsgPrevious; /*!< Previous Request Power Data Object message to be sent */
 uint32_t DPM_RcvRequestDOMsg; /*!< Received request Power Data Object message from the port Partner */
 volatile uint32_t DPM_ErrorCode; /*!< USB PD Error code */
 volatile uint8_t DPM_IsConnected; /*!< USB PD connection state */
 uint16_t DPM_CablePDCapable:1; /*!< Flag to keep information that Cable may be PD capable */
 uint16_t DPM_CableResetOnGoing:1; /*!< Flag to manage a cable reset on going */
 uint16_t DPM_Reserved:15; /*!< Reserved bytes */
 USBPD_SDB_TypeDef DPM_RcvStatus; /*!< Status received by port partner */
#if defined(USBPDCORE_SNK_CAPA_EXT)
 USBPD_SKEDB_TypeDef DPM_RcvSNKExtendedCapa; /*!< SNK Extended Capability received by port partner */
#endif /* USBPDCORE_SNK_CAPA_EXT */
 USBPD_GMIDB_TypeDef DPM_GetManufacturerInfo; /*!< Get Manufacturer Info */
 volatile uint16_t DPM_TimerAlert; /*!< Timer used to monitor current and trig an ALERT */
 USBPD_ADO_TypeDef DPM_SendAlert; /*!< Save the Alert sent to port partner */
 USBPD_ADO_TypeDef DPM_RcvAlert; /*!< Save the Alert received by port partner */
#if defined(_GUI_INTERFACE)
 volatile uint16_t DPM_TimerMeasReport; /*!< Timer used to send measurement report */
#endif /* _GUI_INTERFACE */
 USBPD_DiscoveryIdentity_TypeDef VDM_DiscoCableIdentify; /*!< VDM Cable Discovery Identify */
} USBPD_HandleTypeDef;

This structure is an user structure to be tuned for own USB-PD usage.

Could you please clarify your compilation issues?

At 1st, I can see that the stack library you use is not correct one. For P-NUCLEO-USB002, you have to select 'USBPDCORE_PD3_FULL_CM0_Keil.lib'.

For your information, old applications used for P-NUCLEO-USB002 (MB1303) are available in the package V2.1.0 in github:

=> example of DRP project: https://github.com/STMicroelectronics/x-cube-usb-pd/tree/x-cube-usb-pd-v2.1.0/Projects/STM32F072RB-Nucleo/Applications/USB_PD/MB1303_DRP_RTOS

Regards,

Yohann