2020-06-11 9:40 AM
I 'm using this board for CAN communication with CAN1. I notice in User manual UM1871 Figure 14. MCU 1 CAN1_TX is connected via SB18 and it is open. For CAN1_RX it is mentioned in user manual that I have to close for Rx to work and not mentioned about Tx pin. Do I need to close SB18 for CAN TX to work and it is missed listed in user manual. Please respond.
2020-06-12 6:59 AM
https://www.st.com/en/evaluation-tools/nucleo-f446re.html
[Tab] Resource -> Schematics
https://www.st.com/resource/en/schematic_pack/nucleo_64pins_sch.zip
STM32 Nucleo (64 pins) schematics
You can check the pin connection in the development board circuit diagram.
2020-06-12 7:40 AM
Thank you for your response. I'm using STM32F446E board and not STM32 Nucleo