Skip to main content
SK S.1
Associate III
June 9, 2020
Question

STM32CubeIDE 1.3.0 is not able to connect to Network. Can anyone tell me what maybe the problem?

  • June 9, 2020
  • 8 replies
  • 6941 views

Hi Guys,

I have installed STM32CubeIDE 1.3.0 on my PC which is connected to office network through LAN. Even though  STM32CubeIDE is allowed  to communicate through windows firewall I'm getting network error. One more thing is STM32CubeIDE 1.3.0 is working fine in my development PC which is not connected to the office LAN network.Please go through the attached screenshots to view Network connections and Firewall settings. Can anyone suggest me how to make it work?

With Regards

SUNIL K S

This topic has been closed for replies.

8 replies

Cartu38 OpenDev
Graduate II
June 11, 2020

Is "Help > Eclipse Market place" native Eclipse feature able to fetch material from outside world ?

If no ... please revisit your network settings. If yes let's move to next step then which is to check connection to www.st.com server. Rely on "Windows > Preferences > STM32Cube > Firmware Updater" preference page and have a try pushing "Check Connection" button .. you will have a verdict here ...

SK S.1
SK S.1Author
Associate III
June 22, 2020

​Hi,

Thanks for the reply.

"Help > Eclipse Market place" native Eclipse feature is not able to fetch material from outside world.

I feel some settings in the Firewall or McAfee anti-virus is blocking STM32CubeIDE from connecting to the internet.

I checked with my Networking Team and they are also not able to solve the problem. My IT Team told me that they have allowed the STM32CubeIDE to communicate through windows firewall but still it is not working. What should be the network setting ? Do you have any idea? Please let me know.

With Regards

Sunil K S

Cartu38 OpenDev
Graduate II
June 22, 2020

Are you relying on a proxy ?

My company does. If so you have within network connection preference page to select "Manual" mode as active provider. Then fulfill HTTP & HTTPS stuff.

Takes care never fulfill SOCKS keep it as set by default.

For sure until not able to access to Eclipse Market Place no chance to get access to ST remote material.

SK S.1
SK S.1Author
Associate III
June 24, 2020

​Hi,

Yes I'm relying on proxy server. "Automatically detect" proxy server setting is selected.

I tried with "manual setting" for proxy server but I don't know which IP address and port number should be entered in the entry fields for STM32CubeIDE.

Please refer the attached image for more information.

With Regards

Sunil K S

Cartu38 OpenDev
Graduate II
June 24, 2020

Ok. Unfortunately cannot help you more here. You have to know your proxy setup to allow Eclipse to connect outside. If proxy usage no choice you have to fulfill such "Manual" mode info.

Not expert at all about but maybe such can help : https://superuser.com/questions/346372/how-do-i-know-what-proxy-server-im-using

SK S.1
SK S.1Author
Associate III
June 24, 2020

​Thanks a lot for the help and support.

With Regards

Sunil K S

Rocky
Visitor II
August 14, 2020

Hi,

I encountered same issue then i just reset my windows now working fine.