Skip to main content
kj.obara
Associate III
June 8, 2020
Solved

Nucleo-F446RE board cannot be flashed after being removed without disconnecting removable disk

  • June 8, 2020
  • 2 replies
  • 875 views

Hi, every time that I plug in my Nucleo-F446RE board a removable USB drive also appears (I'm using macOS Catalina 10.15.5). If I unplug the board without unmounting the USB removable disk that appears when it's attached then I have a 90% chance that when I re-plug the board again it will not be recognised properly and I have to restart the whole operating system to make it work again. And I just keep forgetting to remove that USB drive.

So is there any way I can get rid of that functionality entirely? Or any other suggestions how to deal with that? Thank you in advance.

This topic has been closed for replies.
Best answer by waclawek.jan

0693W000001qHUGQA2.png

JW

2 replies

waclawek.jan
waclawek.janBest answer
Super User
June 8, 2020

0693W000001qHUGQA2.png

JW

kj.obara
kj.obaraAuthor
Associate III
June 9, 2020

Oh, I forgot about that. I updated the firmware on the board something like two weeks ago, but I completely forgot about that one.

I'm going to try that and see if it gets rid of the issue. Thank you!