cancel
Showing results for 
Search instead for 
Did you mean: 

Differential ADC to measure voltages above VDD ?

GCho.1
Associate

When using differential ADC, it is safe to to measure voltages above VDD ?

I am trying to measure a voltage different across a current sense resistor from 12VDC power supply.

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
TDK
Super User

No, all voltages need to be within 0 and VREF+.

If you feel a post has answered your question, please click "Accept as Solution".
S.Ma
Principal

The purpose of differential is NOT to have a higher voltage than Vdd. It is to cancel common mode noise. This is also for the same reason that your USB cable is using a differential pair... In the digital world, you can have common voltage higher IF you typically use embedded clock 8b/10b coding AND AC coupling. This is not done on USB nor LVDS, you will find it in Display Port interface.

GCho.1
Associate

Hello,

Thank you for taking time to answer my question. Understood now that sampling voltage should not exceed VDD.

Ozone
Principal III

This trouble is caused by ST's inappropriate use of terms.

A real differential ADC would have an input range spanning positive and negative voltages (e.g. -Vref ... +Vref).

But ST's differential ADC measures the difference between two ADC inputs, while both ADC input potential must be in the range 0V...Vdda.

S.Ma
Principal

Voltages ranges usually are specified in the electrical tables inbdatasheet. TI ADS1299 datasheet do this too.