Question
Project with STM32F439VIT6. After activating Ethernet (DP83848) USB DEVICE CDC (Virtual com port) works not more. Can anybody suggest me where to look?
I make a big project with F439 MCU and there are many things on the board like WiFi, BT, EEPROM, Flash, GPS and so on. The latest thing I made was activating ETH and it works good at least ping runs perfect. But later I found that the USB OTG HS CDC which worked perfectly now doesn't work. Win10 can not recognize the USB divice and Terminal programm can not connect to the port (port is visible some how), firmware freezing. I appreciate any suggestions.