Associate
June 3, 2020
Question
STLINK-V3SET: what pins to connect for the VCP_TX and RX ?
- June 3, 2020
- 2 replies
- 1485 views
Hello.
I am building an application and planning on using the STLINK-V3SET to program and debug, but I can not find any reference which describes what pins to connect for the VCP_TX and RX pins from the programming header to the MCU.
I believe that I connect the following:
T_SWDIO -> PA13
T_SWCLK -> PA14
T_NRST -> NRST
But which pins on the MCU do I connect for the virtual comport?
VCP_TX -> PA2 or PA9
VCP_RX -> PA3 or PA10
Also, SWO is not avaliable on the Cortex M0+? so is not connected?
And other than power and ground no other pins are connected?
Thanks, I found reference to the STLINK-V3 but couldn't find any reference on how to interface with the MCU. Attached are some photos of my schematic.