Skip to main content
CQi.1
Associate
June 3, 2020
Solved

MCSDK 5.4.3/5.4.4. FOC ,Sometimes after encoder alignment ,motor run reverse。

  • June 3, 2020
  • 19 replies
  • 6012 views

Hi!

I have an I-PMSM motor and interfaces an incremental encoder with A B ,without Z.

Sometimes after doing encoder alignment,the motor runs reverse to the max speed,and it will never recover until i do encoder alignment again。

I set the speed 30RPM,but when start ,the motor goes to -200+RPM.

Most time the motor runs well but sometimes the problem will happen.

(STM32 F303VCT6 ;PWM16000KHZ ;Main Sensor :Incremental Encoder2048 no Z-index)

I hope someone could help me figure out the problem.

Best wishes.

This topic has been closed for replies.
Best answer by Bardeen Lai

Hi

  1. Please try to google "initial rotor position alignment method", you could get much more ideas to do proper alignment for incremental encoder. Once you get some ideas, modify the enc_align_ctrl.c, the default ST MCSDK just does the alignment once. However, you could do the alignment again after 10~100ms delay to wait for rotor stable. If your problem still persists, consider to use BDLC with Hall-Effect Sensor, drive it by using 6-steps together with sinusoidal PWM. It would even be less cost concern compared with incremental encoder. The efficiency is not bad, pretty close to FOC but the torque ripple is not as good as the FOC.
  2. Also, you could utilize ST Motor Control Workbench, run the Monitor, try to plot and study some Motor runtime variables, for example, Iq and Id (you should modify the MCI_***)
  3. Use oscilloscope to monitor the Ia, Ib (measured by ADCs), dump these values via DAC or PWM (you have to use RC to do conversion), whether these values look like sinusoidal wave forms
  4. Make sure your 3.3V or 5V DC, pk-pk < 100mV or even lower when the motor is not running. LDO is a good choose but power dissipation is an issue if VBus voltage is higher than 12VDC. I recommend that use DC-DC step down. ST provides many switching IC for this kind of applications.
  5. Again, use RLC filter (band-pass filter) to screen 16KHz ripples from the VBus to your MCU and Encoder

Cheers

19 replies

Laurent Ca...
Senior III
September 14, 2020

Dear CQi.1

Do you have still this problem to solve?

Best regards

Laurent Ca...

intek
Visitor II
September 25, 2020

Hello Laurent Capella

I'm not CQi.1 but I'm having exactly the same problem. Very hard do debug because it happens so rarly. Any hints on where to start or how to resolve this Problem?

Best Regards

Laurent Ca...
Senior III
September 28, 2020

Dear @CQi.1​ , dear @Pascal Klingelhöfer​ 

I do not know if it will help, but according to our "STM32 Forum rules", could you detail your HW configuration (boards, and so on).

Best Regards

Laurent Ca...

ypu
Visitor II
September 29, 2020

Hello Laurent. @Laurent Ca...​ 

I have the same issue and I contacted Japan local team already not yet have the answer

My hardware:

SPIN3201 board, a hub motor, 10 pairs, 340rpm max

start up config:

700ms, 90 degree, 1.95A as default,

use encoder solution, 1024 resolution.

it has about 3% chance that alignment failed in my case. when alignment failed, the speed is -456rpm.

what I can find is that:

when using encoder, the motor started with sensorless, so when I align it to 90 degree, the position the driver got is not that accurate. (maybe sometimes 700ms passed but it has not reach 90 degree, sometimes it just reached and 700ms passed and the rotor moved slight because of initia)

this struck me for about one month.

Laurent Ca...
Senior III
October 14, 2020

Dear @ypu​ 

Did you received answer from ST japan local support team?

Best regards

Laurent Ca...

Bardeen Lai
Associate
October 16, 2020

Hi, there are possible solutions to fix your problem:

  1. The alignment current could be too small, try to increase the alignment current to motor nominal current. Increase even more close to maximum rated motor current if the motor is under heavy load. Besides, you could also fine tune the alignment duration, for example, 2000ms
  2. Depending on the quality of motor, some motor manufacturer could not align the motor properly in the factory, you could modify the FOC high frequency interrupt procedure
void ADC1_2_IRQHandler(void)
{
 ADC1->SR &= ~(uint32_t) (ADC_FLAG_JEOC | ADC_FLAG_JSTRT);
 
 qd_t Iqd, Vqd;
 ab_t Iab;
 SpeednPosFdbk_Handle_t *speedHandle = STC_GetSpeedSensor(pSTC[M1 ]);
 int16_t hElAngle = SPD_GetElAngle(speedHandle) + m_eAngleAdjustment;
.
.
.
}

NOTE: the variable m_eAngleAdjustment is s16degree, you could try to fine tune the electrical angle between -30 to +30 degree which could adjust the encoder vs rotor magnet miss alignment angle.

Hope can you.

Best regards

ypu
Visitor II
October 18, 2020

I did below and the issue does not happen till now.

1. change the duration from 700ms to 2000ms as ST recommended

2. change the current from 1.95A to 7.5A (half of rated current) as ST recommended 

3. directly give a 2V on U-V, and record the position

4. adjust alignment electrical angle, make the rotor the same position as 3, the electrical angle is 60 degrees, then I use " alignment electrical angle = 60 degrees"

With only 1 and 2, the occurrence is lower but the issue still happens sometimes, with 3 and 4, the issue does not happen

Our supplier suggest us to use encoder for speed sensing and Hall sense for commutation, to permanently avoid this risk.

which is not supported originally in  MotorControl Workbench, we would like the explore this option but we would like to know if there is any constraint on the STSPIN3201 hardware side?

regarding your reply 2, high frequency interrupt, I guess you mean high frequency injection?

high frequency injection is not supported in SPIN3201 board (or maybe does not supported in  Workbench 5.4.4).

Bardeen Lai
Associate
October 19, 2020

OK,

Regarding my suggestion 2, you could modify the mc_tasks.c,

/**
 * @brief It executes the core of FOC drive that is the controllers for Iqd
 * currents regulation. Reference frame transformations are carried out
 * accordingly to the active speed sensor. It must be called periodically
 * when new motor currents have been converted
 * @param this related object of class CFOC.
 * @retval int16_t It returns MC_NO_FAULTS if the FOC has been ended before
 * next PWM Update event, MC_FOC_DURATION otherwise
 */
inline uint16_t FOC_CurrControllerM1(void)
{
 qd_t Iqd, Vqd;
 ab_t Iab;
 alphabeta_t Ialphabeta, Valphabeta;
 
 int16_t hElAngle;
 uint16_t hCodeError;
 SpeednPosFdbk_Handle_t *speedHandle;
 
 speedHandle = STC_GetSpeedSensor(pSTC[M1]);
 hElAngle = SPD_GetElAngle(speedHandle) + m_eAngleAdjustment;
 PWMC_GetPhaseCurrents(pwmcHandle[M1], &Iab);
.
.
}

Another suggestion to you, try to modify the enc_align_ctrl.c, make the alignment twice. The angle must be 90 degree applied to Iq (ST default setting)

Your case is pretty weird, have you checked very carefully about the 3.3VDC power source to MCU and the 5VDC power supply to the motor encoder?

The SVPWM produces (MOSFET switching on and off) noises causing the encoder output signals badly. Make sure you have band-pass filters (LCR networks) to screen 16KHz ripples when SVPWM is working. Also, check the encoder output signals whether are differential or TTL.

Finally, when kind of current sensing techniques you are using ICS or 3 R-SHUNT or 1-SHUNT, the power source 3.3VDC to the Op-Amp is crucial. The FOC algorithm runs "crazy" because of bad current sensing feedback.

Honestly speaking, the ST FOC, so far is pretty stable but you have to do some customizations in order suite your working conditions.

Cheers

ypu
Visitor II
October 19, 2020

try to modify the enc_align_ctrl.c, make the alignment twice. The angle must be 90 degree applied to Iq (ST default setting)

  • do you mean both I set to 90 degree? (if the possibility of fail doing once is 1/100​, then doing twice is 1/10000?)
  • is there any reason need to set it to 90 degree? I feel it is "easier" to align it to 60 degree, because that is position when you directly give voltage on U-V

have you checked very carefully about the 3.3VDC power source to MCU and the 5VDC power supply to the motor encoder?

  • I use 5V on motor encoder and added resistor to divide the voltage and also capacitor, the encoder signal is very clean.

The FOC algorithm runs "crazy" because of bad current sensing feedback.

  • that is true, the DCDC of SPIN3201 has some noise, and my issue also happen on ST's evaluation board, I plan to change the DCDC to LDO in my next version.

could explain a little bit more how your suggestion solve the problem when "some motor manufacturer could not align the motor properly"?

Bardeen Lai
Bardeen LaiBest answer
Associate
October 19, 2020

Hi

  1. Please try to google "initial rotor position alignment method", you could get much more ideas to do proper alignment for incremental encoder. Once you get some ideas, modify the enc_align_ctrl.c, the default ST MCSDK just does the alignment once. However, you could do the alignment again after 10~100ms delay to wait for rotor stable. If your problem still persists, consider to use BDLC with Hall-Effect Sensor, drive it by using 6-steps together with sinusoidal PWM. It would even be less cost concern compared with incremental encoder. The efficiency is not bad, pretty close to FOC but the torque ripple is not as good as the FOC.
  2. Also, you could utilize ST Motor Control Workbench, run the Monitor, try to plot and study some Motor runtime variables, for example, Iq and Id (you should modify the MCI_***)
  3. Use oscilloscope to monitor the Ia, Ib (measured by ADCs), dump these values via DAC or PWM (you have to use RC to do conversion), whether these values look like sinusoidal wave forms
  4. Make sure your 3.3V or 5V DC, pk-pk < 100mV or even lower when the motor is not running. LDO is a good choose but power dissipation is an issue if VBus voltage is higher than 12VDC. I recommend that use DC-DC step down. ST provides many switching IC for this kind of applications.
  5. Again, use RLC filter (band-pass filter) to screen 16KHz ripples from the VBus to your MCU and Encoder

Cheers

Associate II
June 25, 2024

why 16kHz ripple?

 

ypu
Visitor II
March 23, 2021

we have finally solved this, we summarized two ways:

  1. run alignment twice to different angle, and count the encoder number, to make sure the motor is aligned in correct position
  2. use encoder for speed measurement and use hall sensor for commutation. (since hall sensor has much less pulse than encoder, so only use hall sensor can not control the motor in low speed)

we finally used 2nd way and it is working fine now.

B.4
Associate
March 30, 2021

Hi @ypu​ ,

I want to try second way, please explain configuration and Connection (like main & auxiliary) of the sensors.

ASaha.3
Associate
April 12, 2023

I am trying to work around this issue by removing the alignment process ,calculating the initial angle required by FOC from the hall sensors. It is working for few angles only. Has anyone tried this yet? Or succeeded to bypass the alignment error issue??

Zain
Associate III
August 1, 2024

Hey,
I am trying to do this exact thing. Have you found any algorithm/solution to this? I need to avoid startup motor running to find index, instead i want to estimate some initial angle and then correct it while i receive index, that will be in one electrical cycle but i want motor to be ready on startup and foc should be working.